It lists all the available channels.
Figure 10-20: Scope Control Panel - Channels




You can change the color of a curve by double-clicking on its color icon, and its visibility by clicking on its check box.
Double-click on any channel in the list to open the Edit all channels dialog box.
When selecting a channel in the channels list, it is superimposed on the existing traces, and some related information are displayed on the left and lower sides of the graph.
It is a tab widget that holds properties related to the channel selected in the list. On some special devices, some more tabs that are specific to extra configurations appear in this widget. For example, S300"Servostar 300 drive" See Servo Drive in Glossary device provides trigger functionalities, so an additional tab is displayed for the trigger configuration.
The current channel properties are:
|
Properties |
Description |
|
Enabled |
A channel has to be enabled to acquire the samples sent by its associated probe |
|
Visible |
A channel has to be visible to be drawn on the graph Even if not visible, it continues to acquire the samples sent by its associated probe |
|
Auto |
A channel in auto mode automatically adapts its amplitude (unit/divisionThe term refers to the time-base value for the X-axis and to the amplitude value for the Y-axis. For example, if the user sets a time-base of 10ms and an amplitude of 1, each division in the soft oscilloscope grid corresponds to a time of 10ms for the X-axis and an amplitude of 1 for the Y-axis.) and zero offset in order to be able to display all its samples. Setting the auto mode disables the possibility of changing the Amplitude and the Zero offset (see Setting Scale for more details about scaling) |
|
Amplitude |
Allows you to control the amplitude |
|
Zero offset |
The curve is vertically shifted so that this value is located halfway through the graph height |
Table 10-4: Scope - Current Channel Properties
Figure 10-21: Scope Control Panel - Current Channel
This enables you to set the speed at which all the lines for each channel are drawn, and is calibrated in milliseconds per division.
Its usage is similar to the Amplitude property described in the above section. The time-base can always be changed, even during sampling (see also Time Scale).
Figure 10-22: Scope Control Panel - Time-base
To setup the time-base properly, the total measurement duration and the required time resolution have to be taken in account.
This enables you to change the time-frame of the acquired samples shown on the graph. It is composed of:
Figure 10-23: Scope Control Panel - Time Position
The acquisition of samples is limited to 100'000 cycles (ie. 100 s when cycle time is set to 1000 µs, and 25 s when cycle time is set to 250 µs). When you reach this limit:
You can change the time slot with the mouse by:


The Time Scale Offset is the time value of the first sample the graph when plotting is started. Using this as an offset, the time axis is always started at 0 seconds. To get the actual time value of any sample, add the time scale offset to the Time axis value.
Actual Sample Time Value = Time Scale Offset + Time axis value
When clicking anywhere on the horizontal line, the time-frame is centered on the clicked point. It is also possible to move the time-frame by clicking on its rectangle part and dragging.
You can resize the time-frame in a user-friendly manner by clicking on its left or right ends and dragging.
During acquisition the time position item is disabled and displays the progression of acquisition.
At the bottom of the controls are five buttons:
allows you to save the acquisition data in a CSV file. For more details, How to Export the Collected Data?.Channel 1: Cycle Jitter (in µs)
When the motion is started, the current cycle time remains constant on an average of several cycles, and equal to the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs cycle time which is a constant value (1000, 500 or 250 µs). The CycleJitterThe difference between the configured cycle time and the actual meausured cycle time. Units in microseconds. is due to EtherCAT transmissions that can vary in a particular cycle (see call out
).
The channel 1 of the scope monitors the time difference between the expected Cycle Time and the actual Cycle Time. (see figure below).
Figure 10-24: Cycle Time Calculation
Channel 2: Motion execution time (microseconds)
Channel 3: PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events execution time (microseconds)
Channel 4: Real Time Margin (microseconds) This channel monitors the available execution time (Cycle Time Period - EtherCAT network execution time - MotionExecTimeThe measured execution time for the Motion Engine (either PipesNetwork or PLCOpen) in each cycle period. Units in microseconds. - PLCProgExecTimeThe measured execution time for the PLC application program (either PipesNetwork or PLCOpen) in each cycle period. Units in microseconds.) in each cycle period.
Figure 10-25: Motion, PLC and Real Time Margin Time Calculations
This feature is not relevant with the KAS Simulator. The MotionExecTime and PLCProgExecTime traces will be visible with simulated values. The CycleJitter and RealTimeMarginThe measured available execution time (equals the Cycle Time Period – EtherCAT network execution time – MotionExecTime – PLCProgExecTime) in each cycle period. Units in microseconds. will always remain at zero with the simulator.
For more explanations, refer to Tasking Model / Scheduling
displays or removes the axis graduations of the graphical area.
changes the time-frame of the graph and amplitudes and zero offsets of channels so that they all fit entirely into the graphical area.
|
Copyright © 2015 Kollmorgen™ |
|